Example Code for Using the TSI-IOBOB2 Scientific Camera Breakout Board with ArduinoThis is example code for using the TSI-IOBOB2 Scientific Camera Break-Out Board with Arduino. Code descriptions are included in the Readme file, and for more information about using the TSI-IOBOB2 in a scientific camera application, please see the user guide on the Support tab. - Example Code: Three samples to give you an idea of the possibilities when combining our TSI-IOBOB2 with an Arduino.
- Support: PDF copy of the TSI-IOBOB2 user guide, which contains more information about setting up and operating the board as a shield for Arduino.
| Support | | |
|---|
| Description | This is the User Guide for the TSI-IOBOB2, containing additional information for setting up the board as a shield for Arduino, as well as information regarding the example programs. |  | | Version | A | | Filesize | 278 KB | | Download | 
Only download from trusted sources, like Thorlabs, and always scan files before executing. | |