Thorlabs Optical Power Monitor Change Log Since Initial Release (V1.0) V6.1 Jul-2024 Bug Fixes: - Prevent to install wrong firmware over ethernet connection. (PM103E, PM5020) V6.0 May-2024 New: - Support for PM60/PM61 Series. Bug Fixes: - PM160 couldn't be connected correctly. (Fixed) - Fast measurement did not work for PM5020. (Fixed) V5.1 Feb-2024 - New: Supports ERM200 Bug Fixes: - Devices with the PID of ERM, SPCNT or some Power meter in the serial number were recognized incorrectly. - User Calibration: three decimal places for the factor. V5.0 May-2023 New: - Support for Single Photon Counter. - I2C functions in TLPMX Driver for PM5020 power meter. - Scope view for PM5020 with a Thermopile. - Sensor Head-Temperature is now display on the measurement view. (Power Meter) - Load PM100D .csv files. Bug Fixes: - Graph Record: Some power meters didn't record the correct measurement type.(e.g. PM160T) (Fixed) - COM ports were not display, if some port was corrupt. (Fixed) V4.1 Nov-2022 New: - Added Script Writer to send "script code" to the PM103. - Command-line tool to communicate with the power meter with SCPI-commands. Bug Fixes: - Edit name and color wasn't visible. (Fixed) - Tuning view for 4Q sensor didn't display dot and position values for PM400 and PM102. (Fixed) - UI freeze on connecting more than two devices on start. (Fixed) - LabView Samples for TLPMX Library were missed. (Fixed) - "Time Out" problem with PM400, PM101 and PM102 solved. V4.0 Jul-2022 New: - Support for PM5020. Bug Fixes: - DFU Driver for PM100USB was not installed. (Fixed) - Values ot of range were set to infinity. (Fixed) - PM103 scope Chart label displays zero for the measurement value. (Fixed) - LabVIEW VIs were not compatible with earlier versions. (Fixed) - PM16x devices can't connect the OPM, when the device use the NI-Visa driver. (Fixed) V3.1 April-2021 Bug Fixes: - Ranges for PM16x Power Meters were display incorrectly. (Fixed) V3.0 March-2021 New features: - Added support for the PM103x power meter interfaces - Zoomt Out Y Axis on right click - Record data in the graph view - Monitoring: Now is possible to set the decimal separator. - Graph\Statistcs View: Now is possible to record the data to the maximal speed of the power meter. - Data Viewer: The data viewer can now load the record data from the graph view. - Help view: Now is possible to set the decimal separator and delimiter for the .csv files. Bug Fixes: - Graph chart slow down on saving 1000 seconds of data. (Fixed) - Rename the device leads to an incorrect behaviour in the monitoring table. (Fixed) Changes: - Monitoring: Minimal interval to save data is now 0.1 seconds - Monitoring: Delimiters list changed. Pilcrow Sign is not supported anymore. V2.2 March-2020 New features: - Added Calibration Wizard for performing user calibrations Bug Fixes: - The OPM installation package installs the USB driver for DFU Mode correctly. - When the firmware update stops due to a time out, the OPM will try to update the firmware again. V2.1 December-2019 New Features: - Added support for the PM102x power meter interfaces - Added support for the S44x thermal position sensors - Integrated Firmware Update Tool into the OPM application - Added Python wrapper class and example for the communication with Thorlabs power meters. Changes: - Help Menu has a new design and functionality. - The selection and search for serial devices was merged with the search for USB devices. V2.0 Aug-2019 Bug Fixes: - For the pyro sensor the NaN values don't increase the samples counter. - The beam size in Y-direction for rectangular beam shape is saved\loaded. - The Graph and Statistics view display the recorded time correctly. - Input Filter state setting is displayed for all power meters with this hardware capability. - For the x axis in the graph view the place between the time stamps is now equidistant. - Application checks for updates if this option was actvated. - PM160/PM16 show the correct range. New Features: - Added support for power meters that use the NI-Visa USB driver - Added support for the PM101x power meter interfaces - Added support for TSP01 and TSP01 rev. B. - Added support for thermopile 4Q sensors - The wavelength value for the PM100USB and PM16 is saved - Each device has now a color indicator in the main view. - Auto Range can be disabled for the PM160/PM16 - A confirmation dialog is opened when the user tries to close the application during logging. Changes: - Statistics\Graph saved files have the same formatting for the numbers as the monitoring file. - Only the selected device can be disconnected from the user interface. V1.1 September-2018 - Adapter type can be selected in the settings.(Adapter) - Trigger Level was added to the settings. (Pyro Sensor) - Bug: Application crash when a device is disconnected. (Fixed) V1.0 March-2018 Initial release